cancel
Showing results for 
Search instead for 
Did you mean: 

BUG report CubeMX V4.15.0, topic: I2S clock calculator

Posted on June 19, 2016 at 14:00

It seems that the clock frequency for the I2S peripheral assumes another clock source (PCLK1 ??) than it should. When PCLK1 is different from SYSCLK this results in erronous calculations.

In the data sheet of the STM32L100 it is specified as follows:

 

''Figure 274 presents the communication clock architecture.. The I2SxCLK source is the system clock (provided by the HSI, the HSE or the PLL, and sourcing the AHB clock).''

2 REPLIES 2
Nesrine M_O
Lead II
Posted on June 20, 2016 at 11:20

Hi Brainport.NL,

Thank you for your feedback. The issue has been reported internally. 

-Syrine-

Sirma Siang
ST Employee
Posted on June 30, 2017 at 17:44

Dear user,

First I would like to thank you for your feedback.

For me the datasheet is correct.

The I2S clock is sysclok.

Then the I2S is connected to a SPI bus for data/registers settings.

Could you please elaborate a bit ?

Kind regards

Sirma