2009-09-15 5:24 AM
Bug in STM32 I2S interface
2011-05-17 4:23 AM
Hello,
I think I have found a bug in the I2S interface of the STM32F103ZE. I have programmed the I2S2 interface in Master Receive PCM Mode. Then, I have tested the four variants shown on figures 227 and 228 of the STM32 Reference manual Rev 9 (page 606). Short frame sync, 16 bits data, 16 bits packet frame : SPI2->I2SCFGR = 0x0F30; OK ! Short frame sync, 16 bits data, 32 bits packet frame : SPI2->I2SCFGR = 0x0F31; OK ! Long frame sync, 16 bits data, 16 bits packet frame : SPI2->I2SCFGR = 0x0FB0; OK ! Long frame sync, 16 bits data, 32 bits packet frame : SPI2->I2SCFGR = 0x0FB1; BAD ! The packet frame is still 16 bits long ! Can somebody confirm that it is a bug ? [ This message was edited by: jcrepetto on 15-09-2009 17:58 ]