Bug in CAN_TransmitStatus function?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-06-10 2:31 PM
I noticed something strange with the CAN_TransmitStatus function in the stm32f10x_can.c (V3.1.2) peripheral driver code. Most of the time it works fine but occasionally it returns the wrong status. The root cause is it’s reading the CANx->TSR register multiple times when updating “state�?. If that register changes between reads, the logic based on “state�? becomes corrupt. The correct way to do this is to first capture CANx->TSR in a local variable then test that value.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-02-13 1:55 AM
I just tumbled on your issue, and I agree that multiple readings of TSR is wrong. I assume that the bit organization inside that register may be leveraged by using 8-bit read depending which mailbox you need to check. An answer from ST about byte access to that register will be appreciated.
Moreover, I suggest that an empty mailbox just return that it is empty and not (as it is currently the case) that transmission failed.