cancel
Showing results for 
Search instead for 
Did you mean: 

BT.656 to RGB

vaidasmikalajunas
Associate II
Posted on April 03, 2014 at 16:26

Hello guys, I've started reading about STM32F429 and start thinking -  if it would be possible to use LCD-TFT controller in such situation:

microcontroller reads BT.656 video signal (8 or 10 bits in parallel + CLK), decode it to normal RGB (24bit - each color 8bits, sync signals, etc...), streams all the data to LCD, plus adds interactive stuf, like clock or date (maby in different layer or transparent). Everything should work at least 30fps. Maby someone was trying to do that and can advice something - or use FPGA in this situation is the only solution?
1 REPLY 1
vaidasmikalajunas
Associate II
Posted on April 14, 2014 at 20:29

any suggestions?