cancel
Showing results for 
Search instead for 
Did you mean: 

Broken Help File - stm32f10x_an3268_fw.chm

lumley
Associate II
Posted on October 05, 2010 at 20:38

I downloaded the firmware package from here:

http://www.st.com/mcu/modules.php?name=mcu&file=devicedocsmdt&FAM=110&DEV=STM32VLDISCOVERY

When I open the file stm32f10x_an3268_fw.chm, the navigation panel appears to work fine (Contents, Index, Search, Favorites). However, the actual pages do not appear -- instead, I get ''Navigation to the wepage was canceled -- Retype the address''.

This happens from two different machines -- workstation and laptop.

Anybody else have this issue?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on October 05, 2010 at 22:27

Seems to work under XP Professional, for the file 981955 bytes, 9/13/2010

Same file fails in manner described in Vista
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jdf25252
Associate II
Posted on October 06, 2010 at 19:40

I get the same thing when trying to open the chm file from a network share.  If you are too, try copying the file to your 'C' drive. (Works for me)  I can get it to work from a USB stick too.  I'm running XP Pro SP3.

jacques23
Associate
Posted on November 05, 2010 at 04:34

right click and go to the proprties of the file, look at read only, security, advanced ...

it worked for me

Andrew Neil
Super User
Posted on November 05, 2010 at 08:51

I think this is a known issue with .chm files - see:

[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/FYI Problems with STM32 Help Files (.chm) and Keil uVision&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&currentviews=149]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fARM%20CortexM3%20STM32%2fFYI%20Problems%20with%20STM32%20Help%20Files%20%28%2echm%29%20and%20Keil%20uVision&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&currentviews=149

See also: 

http://www.keil.com/forum/17404/

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.