cancel
Showing results for 
Search instead for 
Did you mean: 

BOOT1 in STM32L071KZ

ER7
Associate II

Hi

I see there is no boot1 in L071

So bootloader mode is with boot0 = "1" only ?

I'm not missing anything ?​

Thanks

2 REPLIES 2
Uwe Bonnes
Principal III

You miss the option bits. Ther is a nBoot1 option bit!

ER7
Associate II

​Hi

What do you mean by option bit ? can you please explain ? i guess it's not a physical I/O...

I'm asking in means of HW - what do i need to do and how should i approach to the "nBOOT1"

Thanks