cancel
Showing results for 
Search instead for 
Did you mean: 

Boot0/1 & UART1 pins to use

jas
Associate II
Posted on January 23, 2008 at 15:08

Boot0/1 & UART1 pins to use

3 REPLIES 3
jas
Associate II
Posted on May 17, 2011 at 12:22

ST Flash prog utiltity uses USART1

I presume I am NOT allowed to use alternate remapping of pins ?

ie USART1_REMAP = 0

Tx1 has to be on pin PA9 (remap could be PB6)

Rx1 has to be on pin PA10 (remap could be PB7)

Thanks.

[ This message was edited by: Arm_Wrestler on 23-01-2008 16:30 ]

16-32micros
Associate III
Posted on May 17, 2011 at 12:22

Hi,

ST Bootloader is using PA9 and PA10 pins without remap. all of these details will be added in AN2606 version 2. Hope this helps you.

STOne-32

jas
Associate II
Posted on May 17, 2011 at 12:22

Thank you STOne-32