cancel
Showing results for 
Search instead for 
Did you mean: 

Bluetooth module with high speed

Micha? M?ka
Associate
Posted on September 06, 2017 at 09:11

Hello,

I'd like to create signal processing station based on STM F7 MCU and want to send input and processed data using bluetooth to other device. Could you recommend bluetooth module to do such thing? I know, there are BlueNRG, but they work in Bluetooth Low Energy standard and I don't think it will be good for transmitting signal in real time.

#bluetooth
2 REPLIES 2
Zt Liu
Senior III
Posted on September 07, 2017 at 10:09

What is you data rate or throughput? 

If you've not heard of Bluetooh 5 and NRF52, take a look at 

https://devzone.nordicsemi.com/blogs/1078/throughput-and-long-range-demo/

 
Posted on September 08, 2017 at 14:08

I don't know yet, only wondering. I need to have at least 32kBs