2009-07-02 4:36 AM
BLDC sensor based Motor control with the STM8S
2011-05-17 4:16 AM
Hello
I'm searching a motor control library to control a BLDC motor with hall sensors and direct communtation. I'm working on a STM8S and need this library or C-Code as soon as possible. Can you help me? Or do you have a library for the STM32 or another type, so I can modify the code for the STM8S. Thanks a lot Regards, Dominik