Bidirectional Line Termination - will just one resistor work?
I am designing a PCB for an ST micro MCU with external SDRAM.
On the demo board, ST is using one series resistor termination for the bidirectional data lines. ST places this resistor at about 30/70% split of line length, where the resistor is 30 % of line length away from the MCU.
My understanding from research is to use two (2) resistors on bidirectional lines, one at each end, very close to the ICs connected to the line. The resistor values would match the IC output impedance to the line impedance.
What is the general recommended way to terminate a bidirectional data line?
Can a single resistor perform termination on a bidirectional line?