cancel
Showing results for 
Search instead for 
Did you mean: 

backup RAM for STM32H743 device

Anand Ram
Associate III

according to the manual it says 4 Kbytes of backup SRAM in D3.

D3 start address is 0x38000000

in manual address for backup RAM is 0x3880 0000

but below is the behavior observed.

code example.

 __HAL_RCC_BKPRAM_CLK_ENABLE();

 HAL_PWREx_EnableBkUpReg();

 HAL_PWR_EnableBkUpAccess();

by the above code, i can retain the data at address 0x38000000 after the soft reset.

can somebody explain the reason for this.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Pavel A.
Super User

0x38000000 is the D3 SRAM (64 KB)

-- pa

TDK
Super User

> by the above code, i can retain the data at address 0x38000000 after the soft reset.

A soft reset (i.e. a reset without loss of power) won't erase any RAM.

The backup ram can be powered from VBAT which makes it possible to be retained if VDD is lost but VBAT remains.

If you feel a post has answered your question, please click "Accept as Solution".