cancel
Showing results for 
Search instead for 
Did you mean: 

APB2<->AHB1 or APB2<->AHB2 ?

Aleks
Associate III

Hi!

RM0468 "Figure 1. System architecture" show interconnect between APB2/AHB1. But in the DS13311 "Figure 1. STM32H725xE/G" block diagram shown interconnect APB2/ AHB2.

So is there error or there is exactly diagram in DS13311 and generic in RM0468? 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Aleks​ and welcome to the Community :)

Thanks for pointing out this issue. 

The RM0468 is correct: interconnect between APB2/AHB1

I escalated this issue internally to fix the DS13311 in the coming releases.

Please allow me to close this thread, as this will help other users find that answer faster.

Thank you again for having reported the point.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

1 REPLY 1
Imen.D
ST Employee

Hello @Aleks​ and welcome to the Community :)

Thanks for pointing out this issue. 

The RM0468 is correct: interconnect between APB2/AHB1

I escalated this issue internally to fix the DS13311 in the coming releases.

Please allow me to close this thread, as this will help other users find that answer faster.

Thank you again for having reported the point.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen