2014-12-30 6:18 AM
However about TI and Broadcom's BLE 4.0 chipset?
2014-01-02 2:54 PM
I'll offer something a little more useful;
Nordic Semi has the nRF8001 chip, SPI + interrupt interface, but their example code sucks really badly. It would take significant effort to figure out what their code is doing and adapt it to your project. ST has the BlueNRG chip, SPI + interrupt interface, nice looking example code but has a bunch of the Bluetooth stack in a precompiled library. If you aren't using the same compiler as them, and possibly the same target processor family, you may be hooped. (edit: It looks like the stack is built into the BlueNRG chips, so the target system shouldn't be an issue).2014-01-03 1:52 AM
2014-01-04 10:02 AM
I found that nRF51822 is a good BLE 4 chipset. It has a 32-bit Cortex-M0 SoC. I am not sure how difficult to make it work along with STM32F4.
It is better to have all programming just in STM32F4 while a BLE chip is a Bluetooth 4.0 hardware component.2014-01-04 10:04 AM
2014-12-30 7:22 AM
If you're not going to give any specific details of your particular requirements, you might as well just google:
http://www.google.com?q=Bluetooth+Low+Power+Module
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.