2008-06-06 12:48 AM
An2606 rev3 STM32F10xxx system memory boot mode 'STILL' wrong
2011-05-17 3:36 AM
An2606 revision 3 ''STM32F10xxx system memory boot mode'' 'STILL' seems to be wrong.
1) page 9. section Communication Safety. Point 3. (even parity) the hardware I have works with no parity! [incidentally why does the line above end with (XOR=0x00)] 2) page 18. section 2.5 Go Command. A normal human would understand 'the address' to be address to Go from. But in fact you must give the address of a table containing at least two u32. The first u32 should be initial SP. The second u32 should be the initial PC.