2020-05-22 8:46 AM
I have attached the complete log here..
I am trying to use the External mode with Nucle 412 board. But with the above said error.., I am unable to connect to the board at all..,
I initially reported to MATLAB, but they closed the issue stating that it is a STM32 issue., could any one please help me out here..
2020-06-29 5:07 PM
I assume that you have IAR Embedded Worshop installed?
2020-07-30 8:58 AM
I am also having this problem. Any solution to it?
2021-11-17 6:43 PM
I am also having this problem with keil . Any solution to it?
MATLAB 2020b
CubeMX 6.3
STM32 MAT/TARGET 5.6
keil 5.35