cancel
Showing results for 
Search instead for 
Did you mean: 

AI Demo on STM32N6 Discovery Board crashes after some seconds

harald
Associate III

Hy, 

I received the STM32N6 DK Kit, switched it on - and it crashes immediately. All demos run smoothly, but as soon as I start the AI demo, the display turns grey after approx 2 seconds. 

I power the device over USB port with my 65W Laptop Power supply, jumper JP2 set to 3-4 (5V_USB)

When running the DCMIPP_ContinuousMode_FSBL example project, I see a stable, smooth camera image, so apparently no connection issues to the camera.

Any hints?

Best regards

Harald

2 REPLIES 2
Sco
ST Employee

Hello,

there is a similar case which has been discussed, you can refer to: STM32N6570-DK Camera Issue - STMicroelectronics Community

harald
Associate III

Thanks a lot for your response. Reflashing the demo hex file "STM32N6570-DK Out-of-the-box demo binary" from https://community.st.com/t5/stm32-mcus-boards-and-hardware/stm32n6570-dk-camera-issue/td-p/830021 seems to solve the issue. My board is running the AI example properly now.

Regards