2015-01-06 02:06 AM
Hello,
how is the relation between AHBxENR and AHBxLPENR? If some clock is disabled in run-mode, it is automatic also disabled in sleep mode despite the related LPENR bit _not_ reset?. Or is it needed explicit to reset the corresponding bit in the LPENR register to disable in sleep mode even so the corresponding bit is _not_ set in run-mode? I didn't find anything about this in several referenc manuals. #ahbxerr #ahbxlpenr