Adding a second USB port to a STM32L476 based product.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-03 7:32 AM
Posted on October 03, 2017 at 16:32
We need to add a second USB port to a STM32L476 based product so that the produce looks like a USB device to two seperate USB Hosts.
As the STM32L476 has an integrate USB2.0 port, is there a method that add a seperate second USB2.0 port. The product is a audio device and we need to accept audio over USB from two seperate USB hosts.
0 REPLIES 0