ADC3+DMA
I'm having trouble with my STM32h757 processor.
I'm trying to sample 2000 samples using ADC3+DMA1/DMA2/BDMA, but it's not working as expected.
I set up the ADC to work in continuous mode and the DMA to work in circular mode with the address increment set to half-word.
However, when I start the sampling process, the DMA doesn't increment the address and only the first value in the buffer is changing.
I've tried defining the buffer in domain 1, 2, and 3, but it didn't make a difference in the behavior.
IN addition, everything works fine when I use ADC1 instead of ADC3.
Any ideas on what might be causing the issue and how to fix it?
Thanks for your help.