cancel
Showing results for 
Search instead for 
Did you mean: 

ADC Values

yassine
Associate
Posted on March 11, 2015 at 15:03

Hello,

I'm working on the STM32f429i  und i have to program a  game on it using FreeRTOS and uGfx

and i have a Gamepad(Nokia 5110 Gamepad) connected with the STM32f429i.The Buttons are working fine(i used the function GPIO_ReadInputDataBit ) but i have a problem with the Joystik axis.To measure the ADC values of the Joystik  axis  I used the function TM_ADC_Read(ADC3,ADC_Channel4) for the first axis(connected with PF6) and TM_ADC_Read(ADC1,ADC_Channel5) for the second axis(connected with PA5)  but this functions always stop in  while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET) and  while(ADC_GetFlagStatus(ADC3, ADC_FLAG_EOC) == RESET) .this is my code:

static void myTask() {

    font_t font1;

    font1 = gdispOpenFont(''DejaVuSans24*'');

    int x=0,y=0,z=0,e=0,f=0;

    char str[50];

    while(1)

    {

       f=TM_ADC_Read(ADC3,ADC_Channel4);

      e=TM_ADC_Read(ADC1,ADC_Channel5);

        x=GPIO_ReadInputDataBit(RTPL_Register_Buttons,RTPL_Pin_Button_1);

        y=GPIO_ReadInputDataBit(RTPL_Register_Buttons,RTPL_Pin_Button_2);

        z=GPIO_ReadInputDataBit(RTPL_Register_Buttons,RTPL_Pin_Button_J);

        sprintf(str,''But1:%d But2:%d But3:%d J1:%d J2:%d'',x,y,z,e,f);

           gdispClear(White);

        gdispFillString(0,120,str, font1, Red,White);

        vTaskDelay(100);

    }

}

So I decided to do it in another way so i changed the code to this one:

static void myTask() {

    font_t font1;

    font1 = gdispOpenFont(''DejaVuSans24*'');

    int x=0,y=0,z=0,e=0,f=0;

    char str[50];

    while(1)

    {

    TM_ADC_InitADC(ADC1);

    f=ADC_GetConversionValue(ADC3);

    TM_ADC_InitADC(ADC1);

    e=ADC_GetConversionValue(ADC1);

      x=GPIO_ReadInputDataBit(RTPL_Register_Buttons,RTPL_Pin_Button_1);

        y=GPIO_ReadInputDataBit(RTPL_Register_Buttons,RTPL_Pin_Button_2);

        z=GPIO_ReadInputDataBit(RTPL_Register_Buttons,RTPL_Pin_Button_J);

        sprintf(str,''But1:%d But2:%d But3:%d J1:%d J2:%d'',x,y,z,e,f);

           gdispClear(White);

        gdispFillString(0,120,str, font1, Red,White);

        vTaskDelay(100);

    }

}

But then i have  another problem: When i move the Joystik the adc_values don't changes but if i reset the Board they do.So although i use a while loop and i move the Joystik  The ADC_GetConversionvalue always gives the same values and i don't understand why.

PS:Thank you for your Time and I'm sorry for my English

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0