Skip to main content
franck_guillon
Associate
May 16, 2014
Question

ADC result alignment

  • May 16, 2014
  • 4 replies
  • 1153 views
Posted on May 16, 2014 at 04:05

Hello,

I have problem to get the ADC alignment feature working. config: STM32F407 on discovery board, Adjustable voltage (0 to 3V) connected to PA3 ADC resolution set to 12b Whatever alignment setting I use (ADC_DataAlign_Right orADC_DataAlign_Lef), the 4 LSb are always 0 and the result range from 0x0000 to 0xFFF0 for 0 to 3V. The conversion value is right, it just seems that the alignment setting does not have any effect... Does any one has similar issue? Here is my code:

uint32_t ConvResult;
// Initialize ADC
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1,ENABLE);
ADCInitStruct.ADC_Resolution = ADC_Resolution_12b;
ADCInitStruct.ADC_ScanConvMode = DISABLE;
ADCInitStruct.ADC_ContinuousConvMode = DISABLE;
ADCInitStruct.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADCInitStruct.ADC_DataAlign = ADC_DataAlign_Right; // ADC Val max = 4095 @12b resolution
ADCInitStruct.ADC_NbrOfConversion = 1;
ADC_Init(ADC1, &ADCInitStruct);
ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 1, ADC_SampleTime_480Cycles);
ADC_Cmd(ADC1,ENABLE);
// ADC Read
ADC_SoftwareStartConv(ADC1);
while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) != SET);
ConvResult = ADC_GetConversionValue(ADC1);
printf(''%lu: %lx\n'', ConvResult, ConvResult);

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    May 16, 2014
    Posted on May 16, 2014 at 04:31

    Does any one has similar issue?

    The right alignment gives me 0x000..0xFFF

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    franck_guillon
    Associate
    May 16, 2014
    Posted on May 16, 2014 at 04:51

    Hi Clive,

    It's what I was hoping to get, but I get 0x0000 to 0xFFF0 :(...

    Do you see anything wrong on my ADC init code?

    F.

    Tesla DeLorean
    Guru
    May 16, 2014
    Posted on May 16, 2014 at 05:01

    I would hazard that you are not initializing the structure completely, and a side effect of having junk in there is that the ADC gets misconfigured.

    ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
    ADC_InitStructure.ADC_ScanConvMode = DISABLE; // Single Channel
    ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; // Manual Trigger
    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; // NONE
    ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; // VALID BUT NOT USED
    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
    ADC_InitStructure.ADC_NbrOfConversion = 1;
    ADC_Init(ADC1, &ADC_InitStructure);

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    franck_guillon
    Associate
    May 16, 2014
    Posted on May 16, 2014 at 05:12

    Thanks Clive,

    You are right,I did not set the theADC_ExternalTrigConv, and even thought I don't use external trigger, it killed the ADC init. The right alignment works fine now. Here is the corrected code:

    uint32_t ConvResult;
    // Initialize ADC
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1,ENABLE);
    ADCInitStruct.ADC_Resolution = ADC_Resolution_12b;
    ADCInitStruct.ADC_ScanConvMode = DISABLE;
    ADCInitStruct.ADC_ContinuousConvMode = DISABLE;
    ADCInitStruct.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
    ADCInitStruct.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; // Not used but needed for valid init
    ADCInitStruct.ADC_DataAlign = ADC_DataAlign_Right; // ADC Val max = 4095 @12b resolution
    ADCInitStruct.ADC_NbrOfConversion = 1;
    ADC_Init(ADC1, &ADCInitStruct);
    ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 1, ADC_SampleTime_480Cycles);
    ADC_Cmd(ADC1,ENABLE);
    // Conversion
    while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) != SET);
    ConvResult = ADC_GetConversionValue(ADC1);
    printf(''%lu: %lx
    '', ConvResult, ConvResult);

    Thanks again, F.