cancel
Showing results for 
Search instead for 
Did you mean: 

ADC Accuracy

Nitin24
Associate

Dear ST Community,

 I am currently working with the STM32L433RC board, specifically utilizing its 12-bit ADC. Despite my efforts in writing a simple program, I have encountered accuracy issues with errors exceeding 4.5%, and in some instances, even surpassing 30%.

Code :- 

HAL_ADC_Start(&hadc1);

HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);

adc_value = HAL_ADC_GetValue(&hadc1);

float vin = adc_value * (3.3/4095);

sprintf(msg2,"vol = %.3f \r\n",vin);

HAL_UART_Transmit(&huart2, (uint8_t *)msg2, strlen(msg2), HAL_MAX_DELAY);

HAL_Delay(1000);

 

I am also attaching excel sheet to see the difference between Vin and Vout.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Andrew Neil
Super User

@Nitin24 wrote:

I have encountered accuracy issues with errors exceeding 4.5%, and in some instances, even surpassing 30%.


How, exactly, do you measure that?

 

Use this button to properly post source code:

AndrewNeil_0-1706698166984.png

 

To get that extra row of icons, press this button:

AndrewNeil_1-1706698166987.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User

Note that the ADC must be calibrated before it can be used, on every startup.

Note that sampling time tends to be the most important factor--larger sampling times will lead to more accurate values.

See here for general ways to improve accuracy:

https://www.st.com/resource/en/application_note/an2834-how-to-optimize-the-adc-accuracy-in-the-stm32-mcus-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".