cancel
Showing results for 
Search instead for 
Did you mean: 

A simple 2D graphics library for STM32F429 MCU (CooCox project)

peter239955_stm1
Associate
Posted on February 08, 2014 at 19:07

DMA2D accelerated, the sources are here: https://github.com/true-grue/stm32f429_graphics

Tested on STM32F429I-DISCO board with external 480x272 LCD. Hope someone will find it helpful.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
warcatz
Associate II
Posted on February 08, 2014 at 20:38

I see some useful functions in the library.

But i see some thing you can improve , like check if you try to set a pixel out the screen.

This kind of mistake made me crash sometime the st429 :)

It's why i do a clipping.

If you want add other functionality to your lib you can check my source here :

https://sites.google.com/site/suprabotics/source-code

Cheers.

PS : is the st429 fully supported by Coocox now ??

peter239955_stm1
Associate
Posted on February 09, 2014 at 11:14

Thank you for your interest!

To prevent crashing I use bitwise & mask when accessing to the video buffer. Quick and dirty :) I don't know why, but when I use only DMA2D with negative coordinates there is no crashing. I found that it's easier to test the code (for clipping etc) on PC with a SDL-based simulator (it's on github now too) for the graphics library. Also I've added Python scripts for converting png and font (created with BMFont utilty) data to C code.

It's my own, custom CooCox project. It was made with help of flash loader (2 mb support) from here http://olek.tk/blog/index.php?post/2013/11/10/STM32F429I-FLASH-driver-for-CooCox

P.S. I'll check your library soon, thanks for the link!