2017-10-16 01:52 AM
Hi, I have a board with a STM32F103C8T68 (64kb) cpu and I have produced a series of boards with wrong CPU STM32F103CBT6 (128kb).
I have a flash file for the 64 kb edition. Is there an easy way to get the hex file to run on the 128Kb version?
2017-10-16 02:29 AM
Does it not run? Do you have any internal dependencies on the size of the flash sectors?
2017-10-16 04:41 AM
This is a code for a led driver. It receives commands on a com port and drives 3 multi colored LED's with PWM .
The original part was a 64 kb device. We do not have the source code.
I have the programming HEX file from the factory and I can read out the file from a working device.
When I compare files they are all identical.
2017-10-16 07:23 AM
I don't know how complex the application is, perhaps rewriting it is an option.
Or, use gcc based toolchain for ARM, and do a 'objdump' to disassemble the code.
Your name doesn't sound far-eastern, so I guess no IP issues are involved with reverse engineering ... 😉
2017-10-16 08:14 AM
I'll assume you're here because it doesn't work...
The higher functioning part should have more features and do everything the lower part does, the only thing I recall changing/managing on assorted F1 targets was the flash sector sizes.
Have you tried running this on debugger?