cancel
Showing results for 
Search instead for 
Did you mean: 

digital smps - adjustable buck output (B-G474E-DPOW1)

hstetina
Visitor

Hello,

I have a digital buck converter with hrtim. I followed examples Buck_VoltageMode_HW etc. So far so good, output is stable, well regulated to fixed value.

But what if want adjustable output by the user? What is the strategy to do that? I can do a prescaler from feedback ADC to adjust the output, but i feel that it is not the right way to do that properly. 

I'm not well oriented in control theory, but when i set different output voltages in Biricha WDS, control B parameters are slightly different.

 

Unfortunately, I don't have access to bode plot.

What is the proper way to solve this?

  1. Leave B parameters fixed and hope that smps will be stable with different output voltages
  2. Make a lookup table with B parameters for lets say 0,5V steps in output
  3. Calculate b parameters on MCU.
  4. ???

Thank you for the suggestions.

 

Hynek

0 REPLIES 0