2025-03-02 9:59 AM
Hello,
This is my first post here, and just putting it out there from the start, I am no expert in electronics. I am looking for some guidance on putting together a small temperature controller for an EV vehicle conversion. What I am missing is a simple controller that will measure temperatures of two cooling loops and use PWM signals to control two pumps, a heater, and switch on a fan. Below is a more detailed description. BTW if this is not the right place to post this, by all means let me know.
2025-03-02 10:57 AM
is meant to fit into a small enclosure
The Nucleo is OK for a prototype, but production smallness is better achieved with a custom STM32L432 daughterboard, or mounting the micro on the main board. The programming pins would then have to be brought to a connector.
The STM micros have built-in pull up and pull down resistors for the programming pins that are adequate for a benign electromagnetic environment. Consult with an EV EMI expert to determine if your board will need additional programming pull up and pull down resisters to prevent EMI from reprogramming the micro.