2014-06-20 8:40 PM
Hello all,
I,recently?want to migrate application base on library 2.0 of FOC from STM32F103 to STM32F051,and finally found the fowlling error:1:..\Output\svpwm.axf: Error: L6366E: mc_foc_methods.o attributes are not compatible with the provided cpu and fpu attributes .2:..\Output\svpwm.axf: Error: L6366E: mc_state_observer.o attributes are not compatible with the provided cpu and fpu attributes . Want to the help of the predecessors. #foc-2.02014-06-30 11:47 PM
Ciao yongfei.liu
My suggestion is to move to the new version of the MC library that supports STM32F051 Ciao Gigi2014-07-06 6:16 AM
2014-07-14 2:43 AM
Ciao yongfei.liu
I'm sorry, at the moment some parts of the code can't be released with open sources without a signed NDA with the customer and without a real businnes beyond. Ciao Gigi2021-06-28 2:58 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.