cancel
Showing results for 
Search instead for 
Did you mean: 

ST32cubeIDE build error with code generated by Motor control MC_SDK

Thp.1
Associate

Dear all,

I used MotorControl Workbench 5.4.3 to generate code (toolchain st32cubeIDE) and use st32cubeIDE 1.3.0 to build code. If my project is Nucleo IHM001 kit, code build successful. When my project is STEVAL SPIN3202, code build error (collect2.exe: error: ld returned 1 exit status

make: *** [makefile:46: Steval_spin3203_test.elf] Error 1).

Build console:

11:45:45 **** Incremental Build of configuration Debug for project Steval_spin3203_test ****

make all 

arm-none-eabi-gcc -o "Steval_spin3203_test.elf" @"objects.list" -l:libmc-gcc_M0.lib -mcpu=cortex-m0 -T"D:\newpro\Arm\Foc_encoder\firmware_FOC\Steval_spin3202\Steval_spin3203_test\STM32CubeIDE\STM32F031C6TX_FLASH.ld" --specs=nosys.specs -Wl,-Map="Steval_spin3203_test.map" -Wl,--gc-sections -static -L../../MCSDK_v5.4.3/MotorControl/lib --specs=nano.specs -mfloat-abi=soft -mthumb -Wl,--start-group -lc -lm -Wl,--end-group

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: Steval_spin3203_test.elf section `.text' will not fit in region `FLASH'

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: Steval_spin3203_test.elf section `._user_heap_stack' will not fit in region `RAM'

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: region `RAM' overflowed by 8 bytes

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: region `FLASH' overflowed by 22948 bytes

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:46: Steval_spin3203_test.elf] Error 1

"make all" terminated with exit code 2. Build might be incomplete.

11:45:53 Build Failed. 1 errors, 0 warnings. (took 7s.493ms)

How can I fix this error?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Laurent Ca...
Lead II

Dear Thp.1

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Lead II

Dear @Thp.1​ 

I guess you don't have to solve this problem anymore, therefore I consider this post closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...