2015-06-25 12:14 AM
I started to learn to use FOC Lib 4.0 to control a PMSM motor with encoder. I used MC workbench to configure the HW and generated code to SystemDriveParams, then I used the example project for STM32F30x_Workspace.uvmpw since I am using STM32303C-EVAL. Then the project is compiled and downloaded successfully. However, the motor has no response at all. After checking main.c file, I noticed there is no code related with motor control in main(void).
Did I miss anything in the process? How can I make the motor running? #foc2015-06-25 12:44 AM
The entry point of the MC Lib are the MCBoot function in main.c (to create and initialize all relate MC objects) and the Interrupt Service Routine someting in the stm32fxxx_MC_it.c and in Time Base
Ciao Gigi2021-06-27 9:05 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards