Question
Overvoltage fault occures when motor reaches target RPM in FOC SDK V4.3
Hi All,
I am using Nucleo-F302R8 with IHM08M1 power board, 3 shunt mode with hall sensor and FOC SDK V4.3 algorithm. I am able to run my 1KW BLDC motor in Speed control mode. I set the target speed is 3000 RPM. Motor starts and goes upto 3500 RPM and trying to slow down speed, during this time Overvoltage fault stop the motor. My ultimate aim is to drive motor at 6000 RPM in 30 seconds. Kindly guide me to tune the parameters.