cancel
Showing results for 
Search instead for 
Did you mean: 

Issue Running Motor profiler on STM3240G-Eval with STEVAL-IHM028V2.

ASapk
Associate

For our project we want to know the motor parameters of a custom 1.4KW (2HP)Motor. Photo attached.

we are using Motor profiler on STM3240G-Eval with STEVAL-IHM028V2.

The problem is The profiler is failing in its initials stages and not able to identify Rs and Ls.

Its Shows 0 RPM and after some time shows a massage "The measurement is talking two much time"

We have taken care to properly configure boards in motor Control Mode. 

your suggestions Please... 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards