cancel
Showing results for 
Search instead for 
Did you mean: 

How to slove voltage drop ?

Sudhakar.R
Associate III

Hello,

I'm using bldc motor. Battery Voltage is 40.4V. I run the motor on no load the battery voltage is 40.4V and when I apply the load the voltage is dropping.

load(current) is 1A & voltage is 40.3V

load(current) is 2A & voltage is 40.2V

load(current) is 3A & voltage is 40.1V

load(current) is 4A & voltage is 39.9V

how to slove this problem if any one know help me.

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Sudhakar.R
Associate III

our System Design,

I'm working on EV Two wheeler Cluster. I measure the voltage from battery using voltage divider method.

the battery voltage (31 - 40.5) is convert into battery percentage(0 - 99).

In driving time, the voltage is dropping depends on the load. the load is 4A that time the battery is 20 percentage decreas. this is affect the SOC.

LCE
Principal II

For a really good evaluation of battery charge status, you need more than the voltage.

At least know the capacity (Wh), constantly measure voltage and current over time.