How to get a B-G431B-ESC1 to work with an encoder in torque control mode with a pwm input
- April 4, 2020
- 2 replies
- 1333 views
Ill admit that im very fresh when it comes to ST products and software which is probably why Im having trouble.
Im trying to set up a B-G431B-ESC1 essentially like closed loop servo driver.
So far Ive managed to run the motor profiler and started a new project in the motor control workbench but Im getting the following error. When I set the speed sensor to an encoder some of the IO pins seem to be clashing. What I dont get is how to choose which one to use since I cant find a schematic or any reference to which ones should be used. Ive found where to set the controller in torque mode but I cant see where to set the input type.
Assuming I can get past this issue what is the next step to go to to program the controller? The shear amount of programs required is proving hard to get my head around
Thanks