Skip to main content
mcen
Associate
April 22, 2019
Question

How I use the gap drive

  • April 22, 2019
  • 1 reply
  • 582 views

I get the kit STEVAL-HKI001V1 without software, I tryed to use the MotorControl Workbech to generate a code project , and I checked the "use STGAP1S gap drive" like the photo, I builded the project , but failed ,and it prompted that "../MCSDK_v5.2.0-Full/MotorControl/MCSDK/MCLib/Any/Src/gap_gate_driver_ctrl.c(54): error: #5: cannot open source input file "gap_f1f3f4_gate_driver_ctrl.h": No such file or directory" ""no source": Error: #5: cannot open source input file "../MCSDK_v5.2.0-Full/MotorControl/MCSDK/MCLib/F3xx/Src/GAP_F3xx_gate_driver_ctrl.c": No such file or directory", How could I deal it?

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards