cancel
Showing results for 
Search instead for 
Did you mean: 

Can STM32WL be used with STM32Cube.AI ?

Paddykool
Associate

Noob question - can I use AI with the STM32WL SoC ?

I want to train a model and then use STM32Cube.AI to put it on STM32WLE5CC. This is so I can use AI on the end device and transmit data using LoRa all using the one chip.

Is this possible ?

Many thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
fauvarque.daniel
ST Employee

Yes STM32Cube.AI is supported on the STM32WL MCUs

Regards

Daniel

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
fauvarque.daniel
ST Employee

Yes STM32Cube.AI is supported on the STM32WL MCUs

Regards

Daniel

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Paddykool
Associate

Awesome thank you!