cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer does nothing after clicking Start Programming button

BlogOrDie
Associate II

Looking for something to try. I'm want to recover from a failed firmware update of an MLite-880 from Elecevolve after their their 1-click installer. Elecevolve suggested a manual install using the firmware binary and STM32CubeProgrammer. I can put the device in its "DFU FW update mode" and connect to the device from the STM32CubeProgrammer using USB. After connect, the log shows:

08:45:07 : STM32CubeProgrammer API v2.22.0 | Windows-64Bits
08:45:35 : Disconnected from device.
08:46:01 : USB speed : Full Speed (12MBit/s)
08:46:01 : Manuf. ID : MALAHITEAM
08:46:01 : Product ID : Malahit-Lite DFU
08:46:01 : SN : 305B376E3133
08:46:01 : DFU protocol: 1.1
08:46:01 : Board : --
08:46:01 : IAP
08:46:01 : UPLOADING ...
08:46:01 : Size : 1024 Bytes
08:46:01 : Address : 0x8000000
08:46:01 : Read progress:
08:46:01 : Data read successfully
08:46:01 : Time elapsed during the read operation is: 00:00:00.053

When I click Start Programming, literally nothing happens except the progress bar at the bottom previously at 100% clears. Any information as to what these results are telling me, or suggestions as to what to try would be appreciated. I'm using V2.22.0 of STM32Cube Programmer and I have run it from both Windows 10 and 11 computers.

1 ACCEPTED SOLUTION

Accepted Solutions
BlogOrDie
Associate II

There is a postscript to this story. I encountered an expert on flashing the firmware of MAHALIT radios including the MLite-880. He told me that users have variable success using the STM32CubeProgrammer graphic user interface, but that the command line interface always works. I used this plus the binary file name:

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe” -c port=usb1 -d %1 0x08000000 -v 0x08000000 -g 

It worked perfectly and the radio's as good as new.

View solution in original post

10 REPLIES 10
Andrew Neil
Super User

@BlogOrDie wrote:

Elecevolve suggested a manual install using the firmware binary and STM32CubeProgrammer


So have you followed-up with them after their suggestion didn't work?

STM32CubeProgrammer v2.22 has only recently been released - perhaps they rely upon an earlier version?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Employee

Hello @BlogOrDie and welcome to the ST community,

Better to ask Elecevolve directly on support@elecevolve.com

I don't think we can help you here as we don't have information about the STM32 product used inside that MLite-880 device and the hardware adopted.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Elecevolve has made 3 suggestions so far and my question here is at the point of having tried the third suggestion without success. I have replied to them today that it didn't work. From my viewpoint, all of their suggestions are pretty much the same and don't give me confidence that they know what's going on.

I asked here in case the problem is something people see all the time. I realize that it's [edited to add "not"] STM's responsibility.


@BlogOrDie wrote:

I realize that it's STM's responsibility.


No it's not.. as long as we don't know what is inside that device: no MCU part number, no schematics?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I meant to say "not." My apologies for the typo.

 

Andrew Neil
Super User

It seems that this is a brand new consumer product that you have purchased:

https://www.blogordie.com/2026/04/first-impressions-mlite-880-interrupted/

 

So you should do whatever is normal for failed consumer goods in your location.

Here in the UK, it would be the retailers responsibility to fix or replace it.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:

it would be the retailers responsibility to fix or replace it.


Indeed.

@BlogOrDie 

"I meant to say "not." My apologies for the typo.

-> No problem

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
BlogOrDie
Associate II

The manufacturer, Elecevolve, has provided their reply which I paste following in case someone else finds themself in the same situation and ends up here:

We are sorry to hear that the firmware issue remains unresolved. It seems that we will have to wait until the completion of the 1.5 firmware before flashing to that version can finally resolve the problem.

This was a review unit rather than a regular retail purchase, so I'll put it in the box until the new firmware is available.

BlogOrDie
Associate II

There is a postscript to this story. I encountered an expert on flashing the firmware of MAHALIT radios including the MLite-880. He told me that users have variable success using the STM32CubeProgrammer graphic user interface, but that the command line interface always works. I used this plus the binary file name:

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe” -c port=usb1 -d %1 0x08000000 -v 0x08000000 -g 

It worked perfectly and the radio's as good as new.