2024-05-14 01:21 AM
Hello,
I am currently engaged in an IoT project utilizing the STM32H5 microcontroller unit (MCU). I would like to inquire whether the X-CUBE-CELLULAR library is available for the STM32H5 MCU. If it is not currently available, are there any plans to port the X-CUBE-CELLULAR library to the STM32H5 MCU in the future?
Best regards,
2024-05-14 02:12 AM
Hello @Egemen
The last version of the X-CUBE-CELLULAR library gives support for both STM32L4 and STM32U5 as indicated on the Release Note. For the STM32H5, I will escalate your request to the concerned team so they may add the support on the coming versions.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.