What is the difference between I2S_ext_SD and I2S_SD?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-30 8:50 AM
Hello,
Please excuse the basic question, I am reading the datasheet of stm32f429ve trying to understand which pins I need to send data from the microcontroller to an audio codec using I2S.
I understand the I2S interface requires three pins, with an optional fourth pin:
- Bit clock, using PB13 = I2S2_CK
- Word clock, using PB12 = I2S2_WS
- Serial data, using PB15 = I2S2_SD
- Master clock, using PC6 = I2S2_MCK
However, I do not understand the function PB14 = I2S2_ext_SD.
Is this dependent on whether the pin is transmitting or receiving like MOSI or MISO in SPI? I cannot find this documented anywhere which makes me think it must be obvious :)
Solved! Go to Solution.
- Labels:
-
Audio and voice
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-30 9:03 AM
Hi,
read rm ...
So for full duplex I2S you need two data lines : in and out.
Just set it in Cube and you see... or rtfm. :)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-30 9:03 AM - edited ‎2024-04-30 9:04 AM
> I need to send data from the microcontroller to an audio codec using I2S.
Codec means "a combination of ADC and DAC", thus requires data in both directions, i.e. fullduplex ("both MOSI and MISO" in your SPI analogy).
If you need only to *send* from microcontroller, it's then not a *codec* but a DAC. In that case, you need only one data line.
The SPI/I2S module in STM32 is only simplex when it operates in I2S mode, i.e. it has only one data line. To support full-duplex I2S, for some SPI/I2S modules 'F429 (and a few other STM32) incorporate a second, simplified SPI/I2S module called I2Sext, which has only I2S mode (no SPI mode) and its clocks (WS and CK) are internally interconnected to its "partner" SPI/I2S module.
So, if you need fullduplex I2S, you'll need both I2S2_SD and I2S2_ext_SD (and you'll need to set up both SPI2/I2S2 and I2S2ext). If you need only simplex I2S, you don't need I2S2_ext_SD.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-30 9:03 AM
Hi,
read rm ...
So for full duplex I2S you need two data lines : in and out.
Just set it in Cube and you see... or rtfm. :)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-30 9:46 AM - edited ‎2024-04-30 1:33 PM
Thanks for the really helpful advice everyone, that is totally clear. I was searching the PDF and didn’t find that diagram, will be less lazy next time :) because it is not in the data sheet. Instead it is in the Reference Manual RM0090 and appears to be slightly different.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-16 7:26 AM
Hi,
I am a bit late this conversation but I needed an answer to the same question. I get the I2S_ext is a simplified I2S peripheral connected to the I2S/SPI module but my question is how can I configure I2S3_ext peripheral for example_ I can see that it is memory address is 0x4000 4000 - 0x4000 43FF according to the "STM32F427xx STM32F429xx" datasheet but in the reference manual RM0090 there is no mention of configuring I2S_ext modules
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-16 3:07 PM
Configure it in the same way as the "normal" I2S/SPI modules, except that there is no SPI functionality and no I2S Master functionality.
JW