cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual COM Port Driver - is Overlapped IO Mode Supported ?

paulsumpner9
Associate II
Posted on March 14, 2012 at 00:04

We are reading NMEA 0183 data from the USB port of our STM32 based product and our Windows PC Application has been written to use Overlapped IO to minimise performance issues when reading data from lots of COM ports.

The STM32 Virtual COM Port Driver returns an error code when we try to read data using the Overlapped IO functions in Windows, which makes us think that this mode is not supported in the driver. Can anyone confirm if this is true or better still can anyone confirm if they have managed to get the STM32 driver to work in Overlapped IO mode ?

#stm32-virtual-com-overlapped-io
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
tsuneo
Senior
Posted on March 14, 2012 at 17:14

> The STM32 Virtual COM Port Driver

ST supplies just INF file.

The body of the device driver, usbser.sys, is built-in to Windows.

> returns an error code when we try to read data using the Overlapped IO functions in Windows

OVERLAPPED is supported on usbser.sys virtual COM port. There is no difference on coding from usual COM port.

What does GetLastError() return just after ReadFile()?

Tsuneo

paulsumpner9
Associate II
Posted on March 17, 2012 at 00:58

Success, the STM32 Virtual Com Port driver appears like a modem rather than a Com Port and returns a different set of capabilities when queried. It also appears to store and transfer strings of characters rather than individual characters like a Com Port does. We managed to change our application to work around this different way of operating and got it to work in Overlapped IO mode. 

Andrew Neil
Super User
Posted on March 17, 2012 at 02:02

'' ... appears like a modem rather than a Com Port ... ''

 

A ''normal'' Windows modem can be accessed as a COM port, provided you know the COMx: number...

Here's how to find the COMx: number (on XP, at least):

http://blog.antronics.co.uk/2011/09/15/identifying-a-modems-com-port-in-windows-xp/

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on March 18, 2012 at 21:41

It also appears to store and transfer strings of characters rather than individual characters like a Com Port does.

Yeah, I'm not sure what Win32 based COM port's you've been using, but in as long as I can remember you can use ReadData/WriteData to read/write large chunks of data to the COM port, I don't recall ever having to send/receive singular bytes*, with all the overhead that generates. You do have to pay particular attention to what Status, dwRead, and dwWrite return.

* Beyond the obvious conditions where a protocol might only have a single byte to send, only one is pending. ie Dumping whole packets of an XModem-1K @ 460.8Kbaud, and waiting for a single ACK/NACK etc.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..