2026-02-20 3:05 AM
Hello,
I have STM32F7 controller, using Free RTOS, trying to interface external NOR flash, S29GL128S10TFIV13.
I have one source file say testCode.cpp, which I want to move completely in external NOR flash, but every time I ran then code it give Hardfault.
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K
EXT_FLASH (rx) : ORIGIN = 0x64000000, LENGTH = 16M
EXT_SRAM_HEAP (xrw) : ORIGIN = 0x60000000, LENGTH = 256K
EXT_SRAM_STACK (rw) : ORIGIN = 0x60040000, LENGTH = 256K
}
SECTIONS
{
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
.ext_flash_code :
{
. = ALIGN(4);
_sextflash_run = .;
*(.ext_flash_data*)
*(.ext_flash_data*)
. = ALIGN(4);
_eextflash_run = .;
} > EXT_FLASH
/* 2. SECTION FOR MANUAL ATTRIBUTES (For Arrays) */
.ext_flash_data :
{
. = ALIGN(4);
*(.ext_flash_data) /* Targets __attribute__((section(".ext_flash_data"))) */
*(.ext_flash_data*)
. = ALIGN(4);
} > EXT_FLASH
}
Below function I was trying to call from thread,
main()
{
testCodeTaskHandle = osThreadNew(testCodeWrapper, NULL, &testCodeTask_attributes);
}
extern "C"
__attribute__((section(".ext_flash_code")))
void testCodeWrapper(void *argument)
{
testCode* obj = testCode::getInstance();
obj->run();
}Now it gets stuck at first line of this function and then jump to Hardfault.
Note: I have tried to read QRY from flash as test and it PASSED, so flash is integrated correctly.
In .map file it is clearly seen that the function moves to external flash address.
Below init details
hnor2.Instance = FMC_NORSRAM_DEVICE;
hnor2.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
/* hnor2.Init */
hnor2.Init.NSBank = FMC_NORSRAM_BANK2;
hnor2.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hnor2.Init.MemoryType = FMC_MEMORY_TYPE_NOR;
hnor2.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hnor2.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
hnor2.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
hnor2.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hnor2.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hnor2.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
hnor2.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
hnor2.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
hnor2.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
hnor2.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
hnor2.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE;
hnor2.Init.PageSize = FMC_PAGE_SIZE_NONE;
/* Timing */
Timing.AddressSetupTime = 15;
Timing.AddressHoldTime = 15;
Timing.DataSetupTime = 255;
Timing.BusTurnAroundDuration = 15;
Timing.CLKDivision = 16;
Timing.DataLatency = 17;
Timing.AccessMode = FMC_ACCESS_MODE_A;
Help me to understand what is missing here?
Thanks,
Nitin
Solved! Go to Solution.
2026-04-05 9:59 PM
Hello,
As we decided here, I have worked and resolve these 2 issues
External Flash Read/Write: Solved: Re: External NOR Flash Read address line instead o... - STMicroelectronics Community
Move Object to external SRAM: Solved: Re: Move object (.obj) to external SRAM - STMicroelectronics Community
Now everything has works, but additionally as discussed in above thread, I need to work on external Loader application, found support here (https://github.com/STMicroelectronics/stm32-external-loader.git) which has FMC related Loader examples, make sure you correctly configure the pin of FMC for external Loader application as per you project requirements.
Now you have four things to manage:
1. Create a project with external loader and make sure this works using STM32CubeProgrammer, try to edit, delete, read, multi write/read operations on external Flash.
2. Integrate external Loader program to STM32CubeIDE or vscode in main application project, find the reference you can easily find.
"serverArgs": [
"-m", "0",
"-el", "${workspaceFolder}/Loader/testLoader.stldr"
],3. In main application, to access external memory without any limitations (i.e., globally or locally), make sure you initialize FMC and its GPIO inside "SystemInit()" function, that function run at very first stage which make FMC ready for anything.
4. Now, to perform external SRAM operation, you need to copy external/internal FLASH to external SRAM (specifically which execute before main), then make sure you copy external memory to external SRAM and memset to '.bss' sections. And initialize Heap section as mentioned here (Solved: Re: Move object (.obj) to external SRAM - Page 2 - STMicroelectronics Community) So that everything should be ready to run. And that way, it will easily show breakpoint on main(). If you missed anything then you will definitely cause Hard fault before main runs.
Hope my finding helps.
Thanks,
Nitin
2026-02-20 3:15 AM
Hello,
What about this post: External NOR Flash Read address line instead of data?
You need to ensure the read/write is performed without issue to that NOR memory.
2026-02-20 3:16 AM
Did you solve your similar issue: Move object (.obj) to external SRAM ?
2026-02-20 3:19 AM
Hello,
This post External NOR Flash Read address line instead of data? is to simply read/write the flash, and it was failing as explain in that post. But I have tried to read QRY from flash it success, so flash is configure correctly, the only part of flash read/write logic was failing. \
And the current post is about the moving complete object file to external flash, which was also failing.
2026-02-20 3:21 AM - edited 2026-02-20 3:23 AM
Hello,
This is my post only where I was trying to move object in external SRAM, but I didn't get any success.
2026-02-20 3:32 AM
@npatil15 wrote:
Hello,
This post External NOR Flash Read address line instead of data? is to simply read/write the flash, and it was failing as explain in that post. But I have tried to read QRY from flash it success, so flash is configure correctly, the only part of flash read/write logic was failing. \And the current post is about the moving complete object file to external flash, which was also failing.
So how you could continue with this thread if the previous is not solved?
"Now it gets stuck at first line of this function and then jump to Hardfault."
How do you expect to not getting a HardFault while you didn't succeed to read/write to the external NOR flash?
2026-02-20 3:42 AM
@npatil15 wrote:This is my post only where I was trying to move object in external SRAM, but I didn't get any success.
So why not concentrate on getting that working first?
As far as the Linker is concerned, the process would be the same.
As @mƎALLEm said, there are 2 separate issues here:
2026-02-20 3:42 AM
Hello,
I was trying to read/write for testing, just to understand Flash is correctly integrated or not. so, I found one test code which help me to know it is working or not as below
#define NOR_BANK_ADDR ((uint32_t)0x64000000) // Change to 0x60000000 if using NE1
#define ADDR_16(offset) ((__IO uint16_t *)(NOR_BANK_ADDR + ((offset) << 1)))
uint16_t q_char = 0, r_char = 0, y_char = 0;
uint16_t cmd;
*ADDR_16(0x000) = 0x00F0;
HAL_Delay(10);
*ADDR_16(0x55) = 0x0098;
HAL_Delay(10);
// 3. Simple Direct Reads (To rule out your NOR_Read function logic)
q_char = *(__IO uint16_t *)(NOR_BANK_ADDR + (0x10 << 1));
r_char = *(__IO uint16_t *)(NOR_BANK_ADDR + (0x11 << 1));
y_char = *(__IO uint16_t *)(NOR_BANK_ADDR + (0x12 << 1));
RESULT = q_char = 'Q', r_char = 'R', y_char = 'Y'
Now if that post got solution, then that will be my additional knowledge, but if the above script is working then I should move ahead to my actual requirement to use external Flash to move big object/array to external flash.
Thanks
2026-02-20 3:46 AM
Currently I'm not sure does SRAM related object addition is the same as the object addition to Flash. If those are same, then that will be very good, I'm good to focus on SRAM first. If that post has any missing information, then ask me, I will provide that.
Thanks
2026-02-20 3:51 AM
@npatil15 wrote:
I was trying to read/write for testing, just to understand Flash is correctly integrated or not. so, I found one test code which help me to know it is working or not as below
Sorry I didn't understand. Did you solve the read/write operation to the NOR Flash or not? if not, that's not possible to continue in this thread. Again you should solve the previous problem first.