Skip to main content
MPetr.3
Associate II
September 29, 2020
Question

USB Serial communication on STM32L562E-DK

  • September 29, 2020
  • 0 replies
  • 439 views

Hello,

I want to send and receive data between my STM32L562E-DK Discovery Board and my pc via USB.

The best way would be to use the Micro-USB port which also feeds the ST LINK (CN17). Is there an easy way to implement serial receive and send functions? Since this is a standard operation there must be a library present right? Maybe even configurable via the GUI-Configurator in STM32CUBEIDE?

The second option would be the USB-C Port. What is the easiest way to communicate over this port?

(The ultimate goal is to fill the extern OSPI flash with data from the USB port. Getting the data via USB is the only problem here.)

Thanks in advance.

This topic has been closed for replies.