USB OTG HS Host in Mode FS internal PHY and USB OTG FS Device
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-15 10:14 AM
I�m trying to use the STM32F407 as Host and Device simultaneously, my hardware configuration is the following:
-PA12, PA11, PA9 OTG FS as a Device - PB14, PB15 OTG HS as a Host with Embedded PHY If I define the preprocessor symbols: USE_USB_OTG_HS and USE_USB_OTG_FSThe USB works ok as a Host, and the Device goes on and off, It seems that it is going to work but at the end the computer doesn't recognize it. Also, I have tested defining just the preprocessor macro USE_USB_OTG_FS, and in this case the USB works well as a Device. I believe that the library is only implemented to work in HS or FS ModeSo, this is my question, Does any body has implemented USB as a device and host simultaneously using separated peripheral ? I mean i want to use the HS as Host with no external PHY and the FS as a Device. #stm32f4 #usb #usb #usb #usb #stm32f407 #otg #host #host- Labels:
-
STM32F4 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 3:38 AM
Hi
''So, this is my question, Does any body has implemented USB as a device and host simultaneously using separated peripheral ?'' I do not think you can do this! It is not possible (at least with the current USB specification) to have more than 1 host on the USB bus. ie Why would you have the STM32 be a USB Host and a USB device at the same time?!? It is common to have a Composite USB device - that is the STM32 behaves as multiple USB devices eg USB HID and USB CDC together at the same time. The other alternative is called USB OTG - USB On The Go : This allows a 'device' to switch between being a USB Host (ie when the device is not connected to another host and a device is plugged into the STM32 USB) and a USB device (ie when the STM32 is plugged into a USB Host eg PC) This is probably why you see : ''The USB works ok as a Host, and the Device goes on and off''- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 5:55 AM
Thank you Chen_chung,
I would like connect for example: a keyboard or a mouse, and the same time send data to the computer when it is required. Due to your answer I have new Questions: 1.- Can I configure the USB as a Device by default work with this until a condition that makes desinitialize USB, and then Configure the USB as a HOST ? 2.- How Can I implement the USB OTG with different port pins to be able to use Type-A and Type-B Connector at each port pits respectively ? 3. How would you implement this application.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 6:20 AM
Hi
''I would like connect for example: a keyboard or a mouse, and the same time send data to the computer when it is required. '' This is not possible. The STM32 can only be a Host or a Device - it cannot do be both at the same time. To connect to a Keyboard or mouse it must be a Host. To connect to a host computer it must be a Device. '' 1.- Can I configure the USB as a Device by default work with this until a condition that makes desinitialize USB, and then Configure the USB as a HOST ?'' Yes, that is what USB OTG is designed to do. However, it cannot be both at the same time, the STM32 must change over from being a device to host or visa vera. ''2.- How Can I implement the USB OTG with different port pins to be able to use Type-A and Type-B Connector at each port pits respectively ?'' No. The STM32 is only designed to have 1 USB port. This can be either a TypeA (normally for Host) or a TypeB (normally for device). To connect the same port pins to both types of connector would be like connecting the USART port pins to 2x 9w D type - What do you think is going to happen when you connect 2 serial devices to the 1 port? ''3. How would you implement this application.'' What you ask is not possible - cannot be both Host and Device at the same time. The only way to do it is to have 2 USB peripherals - one acting as a Host and one acting as target. I do not think any of the STM32s range have 2 USB peripherals (but I have not really looked either) From the sound of what you have done - you almost have the OTG part working. You just have to make the switch between host/device work.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 6:41 AM
Ok Chen_Chung,
It is helpful. I will try to Implement the USB OTG. But You didn't answer my first question as I want, I mean, I probably can implement this hardware:-PA12, PA11, PA9 OTG FS as a Device
- PB14, PB15 OTG HS as a Host with Embedded PHY
So by software I can Switch between one to other, Initialising the DEVICE (in pins PA12, PA11, PA9) at the first time and then with some hardware/software condition I can turn it Off (Deinitialize it). When it is turned off I will be able to configure the HOST in the other pins. Is it possible? I have read from the Reference Manual that the STM32F407 has two peripherals: USB OTG FS and USB OTG HS, so what I believe is the USB peripherals can work independently once at time. Do I misunderstand the reference manual?... Note: I have understood that I can't use both at the same time.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 7:18 AM
Hi
'' I have read from the Reference Manual that the STM32F407 has two peripherals: USB OTG FS and USB OTG HS, so what I believe is the USB peripherals can work independently once at time. Do I misunderstand the reference manual?... '' Errm - Yes. Maybe you can then. I was under the impression that there is only 1 USB peripheral but looking at the block diagram - they are indeed 2 separate peripherals a Full speed and a High Speed. I do not know?!?. I have not tried it.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-16 7:32 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-01-19 9:05 AM
Bompart.Romy, please keep us updated on your progress. I am wanting to do exactly the same thing - one of the USB ports as host for keyboard or mouse and the other USB port for CDC device to talk to a PC.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-02-23 8:36 AM
Hi Bill,
I did it.. I achieved mix USB OTG HS HOST and USB OTG FS DEVICE. It works Great... !!!- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-03-12 3:24 PM
What did you do to get both a device and host working? I'm running into issues as well and any help would be appreciated.