cancel
Showing results for 
Search instead for 
Did you mean: 

USB MSC write problem

umitguleer
Associate II
Posted on December 29, 2015 at 16:18

Hi everyone,

I have some problem with my STM32F105RC board.for USB MSC application.

I can write usb stick perfectly but some usb is problem and I can not write. That's why 

USB always busy with something and I take a communication error from my modbus designed. I think, it is always here;

static void BSP_Delay(uint32_t nTime, uint8_t unit)

{

  

  BSP_delay = nTime;

  BSP_SetTime(unit);  

  while(BSP_delay != 0);

  TIM_Cmd(TIM2,DISABLE);

}

so can you give me some advice??

#stm32f105rc #usb-msc
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on December 30, 2015 at 01:33

You'd have to dig into whether the timer is setup/enabled, and if variables here are volatile. Evaluate what it's using the delay for.

My preference would be to setup the timer to free run, and mark time against the count.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..