2014-06-12 10:33 PM
Finally find the way out of the Keyboard LEDs working. I use STM32F4 disc with STM32Cube_FW_F4_V1.1.0 and STM32CubeMX 4.2
The HID keyboard program is modified from HID Mouse program
...
static uint8_t USBD_HID_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum);
...
USBD_ClassTypeDef USBD_HID =
{
USBD_HID_Init,
USBD_HID_DeInit,
USBD_HID_Setup,
NULL, /*EP0_TxSent*/
NULL, /*EP0_RxReady*/
USBD_HID_DataIn, /*DataIn*/
USBD_HID_DataOut, /*DataOut*/
NULL, /*SOF */
NULL,
NULL,
USBD_HID_GetCfgDesc,
USBD_HID_GetCfgDesc,
USBD_HID_GetCfgDesc,
USBD_HID_GetDeviceQualifierDesc,
};
__ALIGN_BEGIN static uint8_t USBD_HID_CfgDesc[USB_HID_CONFIG_DESC_SIZ] __ALIGN_END =
{
0x09, /* bLength: Configuration Descriptor size */
USB_DESC_TYPE_CONFIGURATION, /* bDescriptorType: Configuration */
USB_HID_CONFIG_DESC_SIZ,
/* wTotalLength: Bytes returned */
0x00,
0x01, /*bNumInterfaces: 1 interface*/
0x01, /*bConfigurationValue: Configuration value*/
0x00, /*iConfiguration: Index of string descriptor describing
the configuration*/
0xE0, /*bmAttributes: bus powered and Support Remote Wake-up */
0x32, /*MaxPower 100 mA: this current is used for detecting Vbus*/
/************** Descriptor of Joystick Mouse interface ****************/
/* 09 */
0x09, /*bLength: Interface Descriptor size*/
USB_DESC_TYPE_INTERFACE,/*bDescriptorType: Interface descriptor type*/
0x00, /*bInterfaceNumber: Number of Interface*/
0x00, /*bAlternateSetting: Alternate setting*/
0x02, /*bNumEndpoints*/
0x03, /*bInterfaceClass: HID*/
0x01, /*bInterfaceSubClass : 1=BOOT, 0=no boot*/
0x01, /*nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse*/
0, /*iInterface: Index of string descriptor*/
/******************** Descriptor of Joystick Mouse HID ********************/
/* 18 */
0x09, /*bLength: HID Descriptor size*/
HID_DESCRIPTOR_TYPE, /*bDescriptorType: HID*/
0x11, /*bcdHID: HID Class Spec release number*/
0x01,
0x21, /*bCountryCode: Hardware target country*/
0x01, /*bNumDescriptors: Number of HID class descriptors to follow*/
0x22, /*bDescriptorType*/
HID_MOUSE_REPORT_DESC_SIZE,/*wItemLength: Total length of Report descriptor*/
0x00,
/******************** Descriptor of Mouse endpoint ********************/
/* 27 */
0x07, /*bLength: Endpoint Descriptor size*/
USB_DESC_TYPE_ENDPOINT, /*bDescriptorType:*/
HID_EPIN_ADDR, /*bEndpointAddress: Endpoint Address (IN)*/
0x03, /*bmAttributes: Interrupt endpoint*/
HID_EPIN_SIZE, /*wMaxPacketSize: 8 Byte max */
0x00,
0x0A, /*bInterval: Polling Interval (10 ms)*/
/* 34 */
0x07, /*bLength: Endpoint Descriptor size*/
USB_DESC_TYPE_ENDPOINT, /*bDescriptorType:*/
HID_EPOUT_ADDR, /*bEndpointAddress: Endpoint Address (OUT)*/
0x03, /*bmAttributes: Interrupt endpoint*/
HID_EPOUT_SIZE, /*wMaxPacketSize: 1 Byte max */
0x00,
0x0A, /*bInterval: Polling Interval (10 ms)*/
/* 41 */
} ;
...
__ALIGN_BEGIN static uint8_t HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE] __ALIGN_END ={
0x05, 0x01, // USAGE_PAGE (Generic Desktop)
0x09, 0x06, // USAGE_PAGE (Keyboard)
0xa1, 0x01, // COLLECTION (Application)
0x05, 0x07, // USAGE_PAGE (Keyboard)
0x19, 0xe0, // USAGE_MINIMUM (Keyboard LeftControl)
0x29, 0xe7, // USAGE_MAXIMUM (Keyboard Right GUI)
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x25, 0x01, // LOGICAL_MAXIMUM (1)
0x75, 0x01, // REPORT_SIZE (1)
0x95, 0x08, // REPORT_COUNT (8)
0x81, 0x02, // INPUT (Data,Var,Abs)
0x75, 0x08, // REPORT_SIZE (8)
0x95, 0x01, // REPORT_COUNT (1)
0x81, 0x01, // INPUT (Cnst,Ary,Abs)
0x19, 0x00, // USAGE_MINIMUM (Reserved (no event indicated))
0x29, 0x65, // USAGE_MAXIMUM (Keyboard Application)
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x25, 0x65, // LOGICAL_MAXIMUM (101)
0x75, 0x08, // REPORT_SIZE (8)
0x95, 0x06, // REPORT_COUNT (6)
0x81, 0x00, // INPUT (Data,Ary,Abs)
0x05, 0x08, // USAGE_PAGE (LEDs)
0x19, 0x01, // USAGE_MINIMUM (Num Lock)
0x29, 0x03, // USAGE_MAXIMUM (Scroll Lock)
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x25, 0x01, // LOGICAL_MAXIMUM (1)
0x75, 0x01, // REPORT_SIZE (1)
0x95, 0x03, // REPORT_COUNT (3)
0x91, 0x02, // OUTPUT (Data,Var,Abs)
0x75, 0x05, // REPORT_SIZE (5)
0x95, 0x01, // REPORT_COUNT (1)
0x91, 0x03, // OUTPUT (Cnst,Var,Abs)
0xc0 // END_COLLECTION
};
...
static uint8_t rx_buf;
static uint8_t USBD_HID_Init (USBD_HandleTypeDef *pdev,
uint8_t cfgidx)
{
uint8_t ret = 0;
/* Open EP IN */
USBD_LL_OpenEP(pdev,
HID_EPIN_ADDR,
USBD_EP_TYPE_INTR,
HID_EPIN_SIZE);
/* Open EP OUT */
USBD_LL_OpenEP(pdev, HID_EPOUT_ADDR, USBD_EP_TYPE_INTR, HID_EPOUT_SIZE);
pdev->pClassData = USBD_malloc(sizeof (USBD_HID_HandleTypeDef));
//set EP_OUT 1 prepared to received the data
USBD_LL_PrepareReceive(pdev, HID_EPOUT_ADDR, &rx_buf, 1);
if(pdev->pClassData == NULL)
{
ret = 1;
}
else
{
((USBD_HID_HandleTypeDef *)pdev->pClassData)->state = HID_IDLE;
}
return ret;
}
...
static uint8_t USBD_HID_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum){
HAL_PCD_EP_Receive(hUsbDeviceFS.pData, HID_EPOUT_ADDR, &rx_buf, 1);
if (rx_buf & 0x01){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
}
else{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
}
if (rx_buf & 0x02){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
}
else{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
}
if (rx_buf & 0x04){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
}
else{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);
}
return USBD_OK;
}
#define HID_EPIN_ADDR 0x81
//#define HID_EPIN_SIZE 0x04
#define HID_EPIN_SIZE 0x08
#define HID_EPOUT_ADDR 0x01
#define HID_EPOUT_SIZE 0x01
//#define USB_HID_CONFIG_DESC_SIZ 34
#define USB_HID_CONFIG_DESC_SIZ 41
#define USB_HID_DESC_SIZ 9
//#define HID_MOUSE_REPORT_DESC_SIZE 74
#define HID_MOUSE_REPORT_DESC_SIZE 65
#define HID_DESCRIPTOR_TYPE 0x21
#define HID_REPORT_DESC 0x22
Hopefully this could give you a help!
#stm32f4 #usb #discovery
2014-11-06 2:16 AM
Hello leo,
I also tried with the code. But it didn't work. Can you please help me out with some suggestion? Thank you.2024-02-04 11:25 AM
Thanks a lot for sharing!
Here I am10 years after you, struggling with the exact same issue and you helped me greatly with your code snippet.
For those who stumble here my error was that I forgot to set the number of endpoints to 2 in the interface part of the config descriptor:
0x02, /*bNumEndpoints*/
Also, do not put too much processing in much processing in the USBD_HID_DataOut function.
I chose to only write data to rx_buf and process it elsewhere.
Cheers!