cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to debug application running from external PSRAM

Kubis438
Associate

Hello everyone.

In a couple of past days I was trying to make the code execution from external PSRAM to work. I managed to load the code into external FLASH and then copy it to PSRAM at boot stage. The code runs nice but can't debug it for some reason. Debugging worked when I was running the code directly from external FLASH but when I introduced copying the data to PSRAM and running it from there I started to get errors. It wont even let me Run the program if I dont exit the debugger.

Snímka obrazovky 2025-12-02 172139.png

Snímka obrazovky 2025-12-02 172143.png

Snímka obrazovky 2025-12-02 201642.png

I don't understand how it can't access the memory despite the application running fine.

0 REPLIES 0