2019-02-04 11:40 PM
Hello,
I am using a F413ZHTx Controller on a custom board. I am logging data onto the SD card using SDIO interface.
Since I am logging a lot of data, I created a code to:
1) Open the file on the SD card
2) Log 100 entries
3) Close the SD card file
4) Reopen the file.
5) Using f_lseek move to the last location and try appending data.
However, this is still resulting in data being overwritten every 100 entries instead on appending.
Here is my source code:
FRESULT fr;
uint testbyte;
if(f_mount(&myFATFS, "0:" , 1) == FR_OK)
{
// open_append(&myFILE0, "log.csv");
f_open(&myFILE0, "log.csv", FA_WRITE | FA_OPEN_APPEND);
}
count = preload_count;
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);
HAL_CAN_Start(&hcan1);
CAN_Filter_IDList(ID_00, ID_01, 0, 0, ENABLE);
// CAN_Filter_IDList(ID_02, ID_03, 0, 0, ENABLE);
// CAN_Filter_IDList(ID_04, ID_05, 0, 0, ENABLE);
// CAN_Filter_IDList(ID_06, ID_07, 0, 0, ENABLE);
// CAN_Filter_IDList(ID_08, ID_09, 0, 0, ENABLE);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
if(Received_00)
{
// char data1[] = "Inside\n";
// HAL_UART_Transmit(&huart7, (uint8_t*)data1, sizeof(data1), 500);
Received_00 = 0;
count--;
if(count < preload_count && count > 0)
{
// open_append(&myFILE0, "log.csv\0");
sprintf(CANdata,"0x%X, %d | %d | %d | %d | %d | %d | %d | %d\n", RxMessage.ExtId, RxMessage_Data[0], RxMessage_Data[1], RxMessage_Data[2], RxMessage_Data[3], RxMessage_Data[4], RxMessage_Data[5], RxMessage_Data[6], RxMessage_Data[7]);
fr = f_write(&myFILE0, CANdata, strlen(CANdata), &testbyte);
CAN_Filter_IDList(ID_00, ID_01, 0, 0, ENABLE);
char data2[] = "count\n";
HAL_UART_Transmit(&huart7, (uint8_t*)data2, sizeof(data2), 500);
}
else if(count == 0)
{
char data3[] = "100 Written\n";
HAL_UART_Transmit(&huart7, (uint8_t*)data3, sizeof(data3), 500);
f_close(&myFILE0);
CAN_Filter_IDList(ID_00, ID_01, 0, 0, ENABLE);
count = preload_count;
}
else if(count == preload_count)
{
char data1[] = "Next 100\n";
HAL_UART_Transmit(&huart7, (uint8_t*)data1, sizeof(data1), 500);
f_open(&myFILE0, "log.csv", FA_WRITE | FA_OPEN_APPEND);
f_lseek(&myFILE0, f_size(&myFILE0));
// open_append(&myFILE0, "log.csv");
CAN_Filter_IDList(ID_00, ID_01, 0, 0, ENABLE);
}
}
/*****************************************************************************/
/*I also tried using the open_append function I found on ELM_CHAN website, but it didn't work for me.*/
/* USER CODE BEGIN 4 */
FRESULT open_append (
FIL* fp, /* [OUT] File object to create */
const char* path /* [IN] File name to be opened */
)
{
FRESULT fr;
/* Opens an existing file. If not exist, creates a new file. */
fr = f_open(fp, path, FA_WRITE | FA_OPEN_ALWAYS);
if (fr == FR_OK) {
/* Seek to end of the file to append data */
fr = f_lseek(fp, f_size(fp));
if (fr != FR_OK)
f_close(fp);
}
return fr;
}
/* USER CODE END 4 */
Solved! Go to Solution.
2019-02-05 1:10 AM
Hello,
I solved the issue. The issue was not of the SDIO interface but my logic for count.
Thanking You.
2019-02-05 12:11 AM
Try f_lseek() to set the file pointer to the end before writing.
The OPEN_APPEND flag names a capability, not an automatism.
2019-02-05 12:19 AM
Hello AvaTar,
This section of the code does the same thing. After the first preload_count entries are written, then the preload_count is loaded back into the count variable and then I open the file again and perform f_lseek first before writing into the file.
Should I add a f_lseek to the first time I am creating or opening the file?
else if(count == preload_count)
{
char data1[] = "Next 100\n";
HAL_UART_Transmit(&huart7, (uint8_t*)data1, sizeof(data1), 500);
f_open(&myFILE0, "log.csv", FA_WRITE | FA_OPEN_APPEND);
f_lseek(&myFILE0, f_size(&myFILE0));
// open_append(&myFILE0, "log.csv");
CAN_Filter_IDList(ID_00, ID_01, 0, 0, ENABLE);
}
2019-02-05 1:10 AM
Hello,
I solved the issue. The issue was not of the SDIO interface but my logic for count.
Thanking You.
2019-02-05 1:19 AM
Didn't mess much with FATFS recently, but the usual clib way is calling fseek(..,..,SEEK_END) after opening the file. Your code looks fine, have you tried to debug it ?
I use to stick to simple use cases - like write- only, one file per session, file name created from date/time.
And since I mostly write medium-sized strings at a lower rates, I call f_sync() after each write.
FATFS is a limited replacement for the clib. I use to write persistant data from a MCU application, to evaluate them "offline" on a PC.
2019-02-05 1:42 AM
Nice. I did not read up properly on what f_sync does. Now I realize Why I am even closing the file at all when I can simply use the f_sync function.
Thanks @Community member