2013-11-13 01:54 AM
Hi everybody,
I was very happy to see uCLinux port for Cortex-M4 and my favorite MCU STM32. This well done job was achieved by emcraft. So I wonder that is it possible to run uCLinux on my new toy STM32F429I-DISCO? I have started for it and some u-boot and kernel patching I finished my first job. You must known that code execution from SDRAM on STM32F4 much slower than from FLASH (~6x times slower). So in fact this core is not suitable code execution from SDRAM. But maybe you don't have any chance so you can accept this penalty. Than I modified the kernel to load romfs from flash, simple frame buffer driver, u-boot patching for SDRAM and LCD init functions. You can try and decide for yourself. This is boot-up and simple framebuffer demo video. Emcraft original source git is https://github.com/EmcraftSystems (not including STM32F429I-DISCO board drivers)Sample image attached to the post. This image contains u-boot, kernel and romfs. The serial console is USART3 and PC10->MCU TX, PC11->MCU RX. Don't forget that this interface has TTL levels. #usart #stm32-uclinux-u-boot #usb-driver-p19-stm324f2013-11-20 12:41 PM
Very cool!
Is it roughly a 9sec bootup time to command line? It's hard to see from the fuzzy youtube video :-) Emcraft's STM32F4 board gets to the command line in 1sec: http://www.youtube.com/watch?v=_uO8KfhfY2Y Looking forward to playing with this...any known problems with your port and do you plan to contribute the changes back to emcraft?2013-11-22 07:50 AM
2013-11-27 04:04 AM
Hello
Great work :-) Hex work excellent in my DISCO board. You can share source code?2013-11-27 05:17 AM
Great job!!!
I tryed it ...and it works properly. You can share the code??? Congratulations againRegards
2013-11-27 08:12 AM
thanks guys,
I will share the source code. Just I am working on some improvement such as XIP for better performance. Coming soon :)2013-11-27 07:15 PM
Hi tmk,
It is great. Would you please share the binary file ? Thanks. I am porting u-boot but it is halt when I load kernel.2013-11-28 07:33 AM
Hi, tmk
Thank you. While SDRAM address is 0x90000000, it isn't 0xD0000000. Best regards, THANH NHI2013-11-28 12:30 PM
Hi guys,
Finally uCLinux with XIP support demo image is ready forSTM32F429I-DISCO. The attached hex file contains, u-boot, kernel and romfs. Kernel and romfs are executed in-place. So both of them never copied to the SDRAM. STM32 Flash execution supports zero-wait state and XIP performance better than SDRAM execution performance about 6 times. You can check this on console message ''Calibrating delay loop... 34 BogoMIPS''. Yes it is true.I removed LCD console feature. So you can't see kernel debug infos on LCD. Console on serial port is still active. You can test framebuffer driver with ''fbtest'' command. Keep hacking... ________________ Attachments : uboot_kernel_romfs.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzZv&d=%2Fa%2F0X0000000bNs%2FwoQKOCWyzT.3BqjJGCBICwo9D1plfC7JUw4SalZqW_Q&asPdf=false2013-11-28 05:42 PM
Nice project, thanks Mr TMK.
Is there linux kernel usb hcd driver for the STM32F4, Emcraft kernel source has usb gadget only ?Regards