2025-08-30 3:18 PM - edited 2025-08-30 3:47 PM
Hello
I am trying to get the STMN32G431 processor to do what I want.
If I set the baudrates 500kB / 2MB and a samplepoint of 87.5% for both and send a CAN packet with FDF and BRS I get after 3 ms:
LastError = Recessive Bit Error and 8 Tx errors
and 2 ms later:
LastError = Recessive Bit Error, 248 Tx errors and Bus OFF !
Sometimes it is also a Dominant Bit Error.
This happens even in Internal loopback mode!
Therefore I set a Tx delay compensation of zero.
But also with other values for Tx delay compensation, it never works.
If I chose the samplepoint up to 85% all is still fine.
But with 87.5% I get a BusOff which is 100% reproducable.
Now comes the strange thing:
HAL_FDCAN_ConfigTxDelayCompensation(&can_handle, 0, 0);
HAL_FDCAN_EnableTxDelayCompensation(&can_handle);
will produce this problem, but with
HAL_FDCAN_DisableTxDelayCompensation(&can_handle);
it suddenly works correctly!
How is it possible that setting a delay of zero is not the same as a delay that is turned off?
Here my settings:
Clock 160 MHz
Nominal baudrate prescaler: 2
Segment 1 = 139
Segment 2 = 20
JSW = 8
Data baudrate prescaler: 5
Segment 1 = 13
Segment 2 = 2
JSW = 1
_____________________
Where can I find a documentation that explains in detail how to calculate the two values that I must pass to
HAL_FDCAN_ConfigTxDelayCompensation ?
I have been googling the whole day now and I have read the existing sparse documentation from ST and I still have absolutely no clue which values to pass to HAL_FDCAN_ConfigTxDelayCompensation ?
And as this compensates a hardware delay I also don't understand why must we not simply specify a fix delay in nanoseconds ?
If the CAN driver chip has a fix delay of 60 ns, I would expect a configuration where I enter 60 ns and that's it.
Why is this so complicated ?
And why is there no documentation how to calculate the values for offset and filter?
I found a posting that says to set the filter to zero and the offset to DataPrescaler * DataTimeSeg1.
But this does not work for 87.5%.
And it does not make sense to me.
The chip does not care about data segment 1.
The CAN bus transceiver chip has a fix hardware delay that never changes.
I would understand to calculate this delay from the clock frequency, but why from segment 1 ?
Can anybody explain me this in detail please?