cancel
Showing results for 
Search instead for 
Did you mean: 

Trying to do arm_fft_fast_f32 256 bin for a 8000Hz sampled data. Taking only 8000 samples i.e. 1sec and diving into segments to do 256 fft. Not working after first iteration.

AChan.3
Associate

So dividing the sampled data and trying ti do each segment fft just like i did in matlab but the problem is the first segment fft is working next to that fft giving strange values. But if the second set/segment is done fft first it gives the right answer. So it means that arm_rfft function givees right answer only for the first time in a program. If I want to use the function multiple times it seems not to work.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0