cancel
Showing results for 
Search instead for 
Did you mean: 

This is my UART receiving project which is used to accept data from docklight. How do I send binary file into this code?

Shilpashree Madhu
Associate III
#include "main.h"
 
/* Private define ------------------------------------------------------------*/
#define FLASH_USER_START_ADDR   ADDR_FLASH_PAGE_16   /* Start @ of user Flash area */
#define FLASH_USER_END_ADDR     ADDR_FLASH_PAGE_255 + FLASH_PAGE_SIZE - 1   /* End @ of user Flash area */
 
#define DATA_64                 'A'
#define DATA_32                 ((uint32_t)0x12345678)
 
/* Private variables ---------------------------------------------------------*/
uint32_t FirstPage = 0, NbOfPages = 0, BankNumber = 0;
uint32_t Address = 0, PAGEError = 0;
__IO uint32_t data32 = 0 , MemoryProgramStatus = 0;
 
uint8_t buff[10] = {255,80,9,7,1,2,3,4,5,6};
uint8_t flag;
uint8_t data[10];
 
/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
 
/* Private functions ---------------------------------------------------------*/
 
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
   HAL_UART_Receive_IT(&huart2, data, sizeof(data));
   flag = 1;
}
 
/**
  * @brief  Main program
  * @param  None
  * @retval None
  */
int main(void)
{
  HAL_Init();
  /* Configure the system clock to 120 MHz */
  SystemClock_Config();
 
  MX_GPIO_Init();
 
  MX_USART2_UART_Init();
 
  HAL_FLASH_Unlock();
 
  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
 
  Address = FLASH_USER_START_ADDR;
 
  while (1)
  {
	  HAL_UART_Receive_IT(&huart2, data, sizeof(data));
	  if(flag == 1)
	  {
	  HAL_UART_Transmit_IT(&huart2,  data, sizeof(data));
	  while (Address < ADDR_FLASH_PAGE_19)
	  {
	  	  for(uint8_t i = 0; i<10 ;i++)
	  	  {
	         if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, data[i]) == HAL_OK)
	         {
	           Address = Address + 8;
	         }
	        else
	         {
	  	     HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_7);
	         }
	      }
	  }
	  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
	  flag = 0;
	  }
  }
 
  HAL_FLASH_Lock();
 
  while (1)
  {
  }
 
}
 
/**
  * @brief  System Clock Configuration
  *         The system Clock is configured as follows :
  *            System Clock source            = PLL (MSI)
  *            SYSCLK(Hz)                     = 120000000
  *            HCLK(Hz)                       = 120000000
  *            AHB Prescaler                  = 1
  *            APB1 Prescaler                 = 1
  *            APB2 Prescaler                 = 1
  *            MSI Frequency(Hz)              = 4000000
  *            PLL_M                          = 1
  *            PLL_N                          = 60
  *            PLL_Q                          = 2
  *            PLL_R                          = 2
  *            PLL_P                          = 7
  *            Flash Latency(WS)              = 5
  * @param  None
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 
  /* Enable voltage range 1 boost mode for frequency above 80 Mhz */
  __HAL_RCC_PWR_CLK_ENABLE();
  HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);
  __HAL_RCC_PWR_CLK_DISABLE();
 
  /* Enable MSI Oscillator and activate PLL with MSI as source */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
  RCC_OscInitStruct.MSIState = RCC_MSI_ON;
  RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
  RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
  RCC_OscInitStruct.PLL.PLLM = 1;
  RCC_OscInitStruct.PLL.PLLN = 60;
  RCC_OscInitStruct.PLL.PLLR = 2;
  RCC_OscInitStruct.PLL.PLLQ = 2;
  RCC_OscInitStruct.PLL.PLLP = 7;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    /* Initialization Error */
    while(1);
  }
 
  /* To avoid undershoot due to maximum frequency, select PLL as system clock source */
  /* with AHB prescaler divider 2 as first step */
  RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
  if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
  {
    /* Initialization Error */
    while(1);
  }
 
  /* AHB prescaler divider at 1 as second step */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
  {
    /* Initialization Error */
    while(1);
  }
}
 
/**
  * @brief USART2 Initialization Function
  * @param None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 115200;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
}
 
/**
  * @brief GPIO Initialization Function
  * @param None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
 
  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_RESET);
  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14, GPIO_PIN_RESET);
 
  /*Configure GPIO pin : PB7 */
  GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_14;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
 
#ifdef  USE_FULL_ASSERT 
void assert_failed(uint8_t *file, uint32_t line)
{
  while (1)
  {
  }
}
#endif
 
void Error_Handler(void)
{
  __disable_irq();
  while (1)
  {
  }
}

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
KnarfB
Super User

A comment on you code: Using HAL_UART_Receive_IT, setting a flag in the HAL_UART_RxCpltCallback, and polling for it makes not much sense. And, I think you are polling it wrong.

Why not using polling here directly (HAL_UART_Receive). And, if you insist using a flag, make it volatile.

Don't know about docklight though. Usually there are protocols like xmodem, ymodem, zmodem used for that.

hth

KnarfB

Hi @KnarfB, actually my problem is I need to flash application bin file to flash memory using UART bootloader,

​

So If I want to use STMCube programmer, what i need to configure in bootloader project for the UART configuration...if u know anything about how to do this please let me know...

TDK
Super User

If you want to use STM32CubeProgrammer, you would jump to the ROM bootloader in your code and let it handle things. I agree that using polling would make things easier here, since that's all your application is doing. There are examples on how to write flash in the CubeMX repository. Get the basics working first, then add in the UART handling.

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Super User

Duplicate:

https://community.st.com/s/question/0D53W00001NTYdLSAX/i-am-trying-to-write-a-bootloader-on-stm32l4r5zi-mcu-that-gets-data-through-the-uart

If you feel a post has answered your question, please click "Accept as Solution".